KL6xxx in 3 byte mode in combination with bus controllers BCxxxx ================================================================= Because of changes in the memory mapping of BCxxxx bus controllers the three byte mode of the KL6xxx serial line interface will not be longer supported. For future projects please only use COMlibBC5B.lb6 in combination with a 5 byte KL6xxx which is shipped as KL6xxx-0020. Every interface KL6xxx can be reconfigured with the KS2000 software: - ENABLE "5 data bytes mapped in bus coupler" - DISABLE "Alternative output"